Magnet-Free Contact-less Sensor Delivers High Accuracy, Easy Customization, and Smaller Weight and Size with Total Stray Field Immunity for Automotive

January 28, 2021

TOKYO, Japan ― Renesas Electronics Corporation (TSE:6723), a premier supplier of advanced semiconductor solutions, today launched its magnet-free IPS2550 inductive position sensor. Featuring improved performance and easy customization, as well as total stray field immunity, and reduced weight and form factor, the IPS2550 is ideal for use as an absolute position sensor for high-speed motor commutation in passenger cars, heavy-duty commercial and off-road vehicles as well as motorbikes. With its optimized bill-of-materials, the new sensor allows customers to cost effectively tailor sensor design for their applications and maximize the performance of the sensor’s accuracy.

Customers can also take advantage of a complete motor commutation solution for traction motors, electronic power steering, starter generators, and other motor applications when combining the new sensor with Renesas microcontrollers (MCUs), gate drivers, and motor drivers.

“We are excited with the response to the new inductive position sensing technology we introduced last June for industrial motors, and we look forward to bringing its advantages to automotive customers with the new IPS2550,” said Christian Wolf, Vice President, Automotive Sensor Business Division at Renesas. “The IPS2550 provides a slimmer and lighter contact-less sensor that continues to deliver the high performance and stability that automotive applications demand combined with the flexibility and ease of customization that enable businesses to manufacture their own resolver or magnetic sensor replacement cost effectively.”

Based on Renesas’ inductive position sensing technology, the magnet-free IPS2550 delivers speeds up to 600 krpm (electrical) and is designed around the motor, accommodating both off-axis (through shaft and side shaft) and on-axis positioning. Customers can match the number of sectors to pole pairs of the motor and cost-effectively boost accuracy compared with alternative sensing technologies. Featuring total stray field immunity, the thin and light sensor also enables easier motor integration and offers the standard materials required for customers to manufacture their own resolver replacement – reducing bill of materials costs. The IPS2550 has been developed according to ISO26262 to support, as a single IC, the most challenging functional safety critical applications, capable of supporting up to ASIL-C(D) system-level requirements.

Key features of the IPS2550 include:

  • High flexibility with scalability based on the number of motor pole pairs, supporting on-axis, off-axis, and side-shaft alignment
  • AEC-Q100 qualified with stable operation in harsh environments and -40° to +160° C ambient temperatures
  • Enhanced accuracy and production stability with sin/cos gain mismatch and offset compensation
  • Up to 600 krpm (electrical) rotational speed

Renesas also offers a variety of off-the-shelf tools that sensor newcomers and motor commutation experts alike can use to easily create tailored and customized sensing elements.

The IPS2550 is the latest member of Renesas’ inductive position sensing portfolio and joins the company’s robust portfolio of devices for automotive applications, which includes MCUs, system on chips (SoCs), analog, and power management to deliver comprehensive solutions. Customers can further accelerate their designs for quicker time to market by implementing the IPS2550 as part of Renesas’ “Winning Combinations” for BLDC Motor Control, which includes the company’s complementary Analog + Power + Embedded Processing (MCUs and SoCs) product portfolios.

Availability

The IPS2550 is available now with prices starting at $4.76 USD per unit in 1,000-unit quantities. The IPS2500STKIT evaluation kit is also available. (Pricing and availability subject to change). For more information, please visit: http://www.renesas.com/ips2550.

About Renesas Electronics Corporation

Renesas Electronics Corporation (TSE: 6723) delivers trusted embedded design innovation with complete semiconductor solutions that enable billions of connected, intelligent devices to enhance the way people work and live. A global leader in microcontrollers, analog, power, and SoC products, Renesas provides comprehensive solutions for a broad range of automotive, industrial, infrastructure, and IoT applications that help shape a limitless future. Learn more at renesas.com. Follow us on LinkedIn, Facebook, Twitter, and YouTube.

(Remarks). All names of products or services mentioned in this press release are trademarks or registered trademarks of their respective owners.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.

Share this news on