Overview

Description

This development assistance tool supports the development of embedded systems which use the camera functions of display controllers from Renesas. It supports MCUs of the RZ family.

Features

  • Easy Settings for the Timing of Input Signals from Cameras
  • Easy Alterations to the Operation of the Camera Module
  • Support for the Debugging of Images Captured by Cameras
  • Check the Results of the Settings on the Actual Camera & Display
  • Generate a Header File Which Reflects the Settings for Use in Projects
  • Learn More

Release Information

Package Component
QE for Camera
Latest Ver.: V1.1.1
Released: Apr 07, 2020
For RZ Family QE for Camera[RZ]
Latest Ver.: V1.1.1
Released: Apr 07, 2020
Operating Environment 
* QE for Display[RZ] is installed along with this product. (Previous product name: QE for Video Display Controller 5)

Download

Installing This Product >>

Target Devices

Downloads

Type Title Date
Software & Tools - Other Log in to Download ZIP 2.45 MB 日本語
1 item

Design & Development

Sample Code

Additional Details

Functions

Easy Settings for the Timing of Input Signals from Cameras

The GUI allows the easy adjustment of the timing settings of a camera during testing. GUI displays with appropriate settings for various RZ/A target boards or custom boards for development are set up by selecting a target board or setting custom board configurations (Note1). The settings corresponding to those in the GUI display are created in a header file for direct incorporation in projects. If the value of a setting is not in accordance with the MCU spec., it is marked as being in error. This makes it easy for users to identify problems.

Note

  1. Only the RZ/A2M supports MIPI-standard cameras.
Image

Easy Alterations to the Operation of the Camera Module

Operation settings such as the image format and capture size of the camera module to be connected can be specified by sending a parameter file (csv file) from QE for Camera.

Image

Support for the Debugging of Images Captured by Cameras

Even for a system that has no display device, such as a surveillance camera, interlinking with the in-memory image display function of the e² studio allows you to check images in the buffers for the VDC5.

Image

Check the Results of the Settings on the Actual Camera & Display

A single button press writes the current settings to registers, so you can check the results for the actual camera and LCD panel. This tool also has a mode for automatically writing the changes to registers every time a setting is changed.

Image

Generate a Header File Which Reflects the Settings for Use in Projects

When you have finished the settings, the settings corresponding to those in the GUI display are created in a header file for direct incorporation in projects. QE for VDC5 can also operate in conjunction with the Supported Sample Programs.

Image

Supported Sample Programs

Product Name Sample Program
QE for Camera[RZ] RZ/A1LU Software Package
RZ/A2M Software Package
RZ/A1H Group, RZ/A1M Group, RZ/A1LU Group, RZ/A1L Group, RZ/A1LC Group RZ/A1 Framework

Target Devices

Product Name Family Series Group
QE for Camera[RZ] RZ RZ/A RZ/A1H, RZ/A1L, RZ/A1LC, RZ/A1LU, RZ/A1M, RZ/A2M