R-Car/Boards/S4SK/Xen-Hypervisor/SDK-v3.16.2
|
Software revisions
Software | Revision |
---|---|
R-Car SDK | v3.16.2 |
R-Car S4 Xen package | version 1.2.1 |
R-Car S4 Linux Yocto package | Based on version 5.24.2 |
Yocto Project | 3.1.16 |
aarch64-poky-linux-gcc (GCC) | 9.3 |
Xen Hypervisor | 4.17-unstable |
Dom0 (Linux kernel) | 5.10.41/rcar-5.1.7.rc12 |
DomD (Linux kernel) | v5.10.41/rcar-5.1.7.rc11.2-xt |
DomU (Linux kernel) | v5.10.41/rcar-5.1.7.rc11.2-xt |
Userland 64/32bit | 64 |
U-Boot | 2020.10 |
Host PC
Ubuntu 20.04 LTS (64bit) is recommended as OS. 32bit version is not supported.
How to build
See also : https://github.com/renesas-rcar/meta-xt-prod-devel-rcar-gen4/blob/s4sk-mp-1.0/doc/building.md
Installation of required tools and libraries
Ubuntu is used as Linux Host PC since Yocto Project Quick Start specifies Ubuntu as one of the distributions. You need to install the required packages as follows.
sudo apt-get install -y gawk wget diffstat texinfo chrpath socat \ libsdl1.2-dev python-crypto checkpolicy python3-git python3-github \ bzr pigz m4 lftp openjdk-8-jdk git-core gnupg flex \ bison gperf build-essential zip curl zlib1g-dev gcc-multilib g++-multilib \ libc6-dev-i386 lib32ncurses5-dev x11proto-core-dev libx11-dev lib32z-dev \ ccache libgl1-mesa-dev libcap-ng-dev libxml2-utils xsltproc unzip \ python-clang-6.0 gcc-7 g++-7 bc python3-pyelftools python3-pip \ python3-crypto libpixman-1-dev libcap-dev device-tree-compiler libffi-dev \ python-dev libgit2-dev ninja-build curl
Using build script
- Build script(build.sh)
#!/bin/bash # Install moulin pip3 install --upgrade pip export PATH="$PATH:${HOME}/.local/bin" pip3 install --user git+https://github.com/xen-troops/moulin # build mkdir build-xen cd build-xen export WORK_XEN=`pwd` curl -O https://raw.githubusercontent.com/renesas-rcar/meta-xt-prod-devel-rcar-gen4/s4sk-1.2.1/prod-devel-rcar-s4sk.yaml moulin prod-devel-rcar-s4sk.yaml --ENABLE_DOMU=yes ninja
- build
./build.sh
Manual steps
- Install moulin
pip3 install --upgrade pip export PATH="$PATH:${HOME}/.local/bin" pip3 install --user git+https://github.com/xen-troops/moulin
- Build
mkdir build-xen cd build-xen export WORK_XEN=`pwd` curl -O https://raw.githubusercontent.com/renesas-rcar/meta-xt-prod-devel-rcar-gen4/s4sk-1.2.1/prod-devel-rcar-s4sk.yaml moulin prod-devel-rcar-s4sk.yaml --ENABLE_DOMU=yes ninja
- Building image can take up to a few hours depending on your host system performance.
After the build has been completed successfully, you should see the output similar to:NOTE: Tasks Summary: Attempted 2734 tasks of which 1752 didn't need to be rerun and all succeeded.
Generated images
- Dom0: ${WORK_XEN}/yocto/build-dom0/tmp/deploy/images/generic-armv8-xt/
- DomD: ${WORK_XEN}/yocto/build-domd/tmp/deploy/images/s4sk/
- DomU: ${WORK_XEN}/yocto/build-domu/tmp/deploy/images/s4sk/
Domain Expected output Description Dom0 Image Dom0 Linux kernel image uInitramfs Dom0 ramfs((Included DomD/U Images and device trees)) DomD rcar-image-minimal-s4sk.tar.bz2 DomD rootfs r8a779f0-s4sk -xen.dtb Xen device trees xenpolicy-s4sk
xen-uImageXen image u-boot-elf-s4sk.srec U-Boot bl31-s4sk.srec Trusted Firmware-A (BL31) tee-s4sk.srec OP-TEE OS DomU rcar-image-minimal-s4sk.tar.bz2 DomU rootfs
- Sample built Image is below.
- https://hydrochoerus.com/rcar/s4sk-xen/build-xen/yocto/
How to flash/update the loader
$ ls -1 ${WORK_XEN}/yocto/build-domd/tmp/deploy/images/s4sk/*.srec yocto/build-domd/tmp/deploy/images/s4sk/bl31-s4sk.srec yocto/build-domd/tmp/deploy/images/s4sk/tee-s4sk.srec yocto/build-domd/tmp/deploy/images/s4sk/u-boot-elf-s4sk-v2020.10+gitAUTOINC+616f05eb5a-r0.srec yocto/build-domd/tmp/deploy/images/s4sk/u-boot-elf-s4sk.srec yocto/build-domd/tmp/deploy/images/s4sk/u-boot-elf.srec
- Write the generated bl31-s4sk.srec, tee-s4sk.srec and u-boot-elf-s4sk.srec binaries to flash
- See : R-Car/Boards/S4SK#How_to_flash.2Fupdate_the_loader
How to boot
Micro SD card(32GB or more) boot
WARNING! These steps will erase the SD card completely. In short, all files will be lost.
Follow these steps on the host machine:
NOTE: probably you need to be a root user, hence use "sudo". And "mmcblk0" should be adapted to your environment (eg., sdb or sdc).
- Delete all the partitions in the SD card. Below is an example for one partition, repeat the process for all the remaining partitions in the SD card if exists.
Ex) $ fdisk /dev/mmcblk0 Command (m for help): d Partition number (2-4, default 1): 1 (number of the first partion) Partition 1 has been deleted.
- Divide the SD card into three partions and set ID=83(Linux) for each.
Ex) $ fdisk /dev/mmcblk0 Command (m for help): n Partition type p primary (0 primary, 0 extended, 4 free) e extended (container for logical partitions) Select (default p): p Partition number (1-4, default 1): 1 (number of the first partion) First sector (2048-62333951, default 2048): <Hit Enter key> Last sector, +/-sectors or +/-size{K,M,G,T,P} (2048-62333951, default 62333951): +9G (Size of the first partion) Created a new partition 1 of type 'Linux' and of size 9 GiB. Partition #1 contains a ext4 signature. Do you want to remove the signature? [Y]es/[N]o: n Command (m for help): t Selected partition 1 Hex code (type L to list all codes): 83 Changed type of partition 'Linux' to 'Linux'.
- Repeat the above commands for the second and third partitions by changing the partition number to 2 and 3.
- Format each partition to ext4
$ mkfs.ext4 /dev/mmcblk0p1 $ mkfs.ext4 /dev/mmcblk0p2 $ mkfs.ext4 /dev/mmcblk0p3
- Write images to partitions of SD card
$ mount /dev/mmcblk0p1 /mnt $ cp ${WORK_XEN}/yocto/build-dom0/tmp/deploy/images/generic-armv8-xt/Image /mnt $ cp ${WORK_XEN}/yocto/build-dom0/tmp/deploy/images/generic-armv8-xt/uInitramfs /mnt $ cp ${WORK_XEN}/yocto/build-domd/tmp/deploy/images/s4sk/r8a779f0-s4sk-xen.dtb /mnt $ cp ${WORK_XEN}/yocto/build-domd/tmp/deploy/images/s4sk/xen-uImage /mnt/ $ cp ${WORK_XEN}/yocto/build-domd/tmp/deploy/images/s4sk/xenpolicy-s4sk /mnt $ sync $ umount /mnt $ mount /dev/mmcblk0p2 /mnt $ tar jxf ${WORK_XEN}/yocto/build-domd/tmp/deploy/images/s4sk/rcar-image-minimal-s4sk.tar.bz -C /mnt $ sync $ umount /mnt $ mount /dev/mmcblk0p3 /mnt $ tar jxf ${WORK_XEN}/yocto/build-domu/tmp/deploy/images/s4sk/rcar-image-minimal-s4sk.tar.bz2 -C /mnt $ sync $ umount /mnt
- Set U-Boot environment variables
setenv initrd_high 0xffffffffffffffff setenv bootargs setenv bootcmd 'run bootcmd_sdcard' setenv bootcmd_sdcard 'run sdcard_xen_load; run sdcard_dtb_load; run sdcard_kernel_load; run sdcard_xenpolicy_load; run sdcard_initramfs_load; bootm 0x48080000 0x84000000 0x48000000' setenv sdcard_dtb_load 'ext4load mmc 0:1 0x48000000 r8a779f0-s4sk-xen.dtb; fdt addr 0x48000000; fdt resize; fdt mknode / boot_dev; fdt set /boot_dev device mmcblk0' setenv sdcard_initramfs_load 'ext4load mmc 0:1 0x84000000 uInitramfs' setenv sdcard_kernel_load 'ext4load mmc 0:1 0x7a000000 Image' setenv sdcard_xen_load 'ext4load mmc 0:1 0x48080000 xen-uImage' setenv sdcard_xenpolicy_load 'ext4load mmc 0:1 0x7c000000 xenpolicy-s4sk' run bootcmd
Tips
Writing an image to Micro SD using the dd command
This frees you from confusing Micro SD partitioning, formatting, and other procedures.
- build (See R-Car/Boards/S4SK/Xen-Hypervisor#How_to_build)
./build.sh
- or
ninja
- Generated the "full.img" file
ninja image-full
ls build.ninja full.img prod-devel-rcar-s4sk.yaml yocto
- Writing the "full.imge" to Micro SD
dd if=full.img of=/dev/mmcblk0 conv=sparse
- Boot
setenv bootargs setenv bootcmd 'ext4load mmc 0:1 0x83000000 boot-emmc.uImage; source 0x83000000' run bootcmd
NFS boot
- Install some packages for NFS boot on Host PC (See R-Car/Boards/Yocto-Gen3/v5.9.0#Loading_kernel_via_TFTP_and_rootfs_via_NFS)
- Copy and decompress the some files and rootfs on Host PC
Ex) $ mkdir -p /srv/tftp/s4/rootfs_xen/dom0 /srv/tftp/s4/rootfs_xen/domd /srv/tftp/s4/rootfs_xen/domu $ export NFS_ROOT=/srv/tftp/s4/rootfs_xen $ cp ${WORK_XEN}/yocto/build-dom0/tmp/deploy/images/generic-armv8-xt/Image ${NFS_ROOT}/dom0 $ cp ${WORK_XEN}/yocto/build-dom0/tmp/deploy/images/generic-armv8-xt/uInitramfs ${NFS_ROOT}/dom0 $ cp ${WORK_XEN}/yocto/build-domd/tmp/deploy/images/s4sk/r8a779f0-s4sk-xen.dtb ${NFS_ROOT}/dom0 $ cp ${WORK_XEN}/yocto/build-domd/tmp/deploy/images/s4sk/xen-uImage ${NFS_ROOT}/dom0 $ cp ${WORK_XEN}/yocto/build-domd/tmp/deploy/images/s4sk/xenpolicy-s4sk ${NFS_ROOT}/dom0 $ tar jxf ${WORK_XEN}/yocto/build-domd/tmp/deploy/images/s4sk/rcar-image-minimal-s4sk.tar.bz -C ${NFS_ROOT}/domd $ tar jxf ${WORK_XEN}/yocto/build-domu/tmp/deploy/images/s4sk/rcar-image-minimal-s4sk.tar.bz2 -C ${NFS_ROOT}/domu
- Set U-Boot environment variables and boot
setenv bootargs setenv bootdelay 2 setenv baudrate 921600 setenv initrd_high 0xffffffffffffffff setenv serverip 192.168.10.111 setenv ipaddr 192.168.10.100 setenv tftp '/s4/rootfs_xen/dom0' setenv rfs '/srv/tftp/s4/rootfs_xen' setenv boot_dev nfs setenv bootcmd_tftp 'run tftp_xen_ld; run tftp_dtb_ld; run tftp_kernel_ld; run tftp_policy_ld; run tftp_ramfs_ld; bootm 0x48080000 0x84000000 0x48000000' setenv tftp_configure_nfs 'fdt set /boot_dev device ${boot_dev}; fdt set /boot_dev my_ip ${ipaddr}; fdt set /boot_dev nfs_server_ip ${serverip}; fdt set /boot_dev nfs_dir ${rfs}/domd; fdt set /boot_dev domu_nfs_dir ${rfs}/domu;' setenv tftp_dtb_ld 'tftp 0x48000000 ${tftp}/r8a779f0-s4sk-xen.dtb; fdt addr 0x48000000; fdt resize; fdt mknode / boot_dev; run tftp_configure_nfs;' setenv tftp_ramfs_ld 'tftp 0x84000000 ${tftp}/uInitramfs' setenv tftp_kernel_ld 'tftp 0x7a000000 ${tftp}/Image' setenv tftp_xen_ld 'tftp 0x48080000 ${tftp}/xen-uImage' setenv tftp_policy_ld 'tftp 0x7c000000 ${tftp}/xenpolicy-s4sk' setenv bootcmd 'run bootcmd_tftp' run bootcmd
Confirmed Xen Commands
Dom0
- Get information about Xen host (xl info)
root@generic-armv8-xt-dom0:~# xl info host : generic-armv8-xt-dom0 release : 5.10.41-yocto-tiny version : #1 SMP PREEMPT Fri Sep 1 06:40:51 UTC 2023 machine : aarch64 nr_cpus : 8 max_cpu_id : 7 nr_nodes : 1 cores_per_socket : 1 threads_per_core : 1 cpu_mhz : 16.666 hw_caps : 00000000:00000000:00000000:00000000:00000000:00000000:00000000:00000000 virt_caps : hvm hvm_directio hap iommu_hap_pt_share vpmu gnttab-v1 total_memory : 3456 free_memory : 1501 sharing_freed_memory : 0 sharing_used_memory : 0 outstanding_claims : 0 free_cpus : 0 xen_major : 4 xen_minor : 17 xen_extra : -unstable xen_version : 4.17-unstable xen_caps : xen-3.0-aarch64 xen-3.0-armv7l xen_scheduler : credit2 xen_pagesize : 4096 platform_params : virt_start=0x200000 xen_changeset : Thu Dec 8 19:01:46 2022 +0000 git:df73c24859-dirty xen_commandline : dom0_mem=256M console=dtuart dtuart=/soc/serial@e6540000 dom0_max_vcpus=2 loglvl=all xsm=flask flask=permissive bootscrub=0 pci-passthrough=on cc_compiler : aarch64-poky-linux-gcc (GCC) 9.3.0 cc_compile_by : xen-4.17.0+gitA cc_compile_domain : poky cc_compile_date : 2022-12-20 build_id : dd12b927ba9ed4a4d0c3af6b7e509e75cfc36124 xend_config_format : 4 root@generic-armv8-xt-dom0:~#
- List information about all/some domains (xl list)
root@generic-armv8-xt-dom0:~# xl list Name ID Mem VCPUs State Time(s) Domain-0 0 256 2 r----- 12.5 DomD 1 1021 4 -b---- 21.0 DomU 2 511 2 -b---- 8.2 root@generic-armv8-xt-dom0:~#
- Terminate a domain immediately (xl destroy DomU)
root@generic-armv8-xt-dom0:~# xl list Name ID Mem VCPUs State Time(s) Domain-0 0 256 2 r----- 12.5 DomD 1 1021 4 -b---- 21.0 DomU 2 511 2 -b---- 8.2 root@generic-armv8-xt-dom0:~# root@generic-armv8-xt-dom0:~# root@generic-armv8-xt-dom0:~# xl destroy DomU root@generic-armv8-xt-dom0:~# xl list Name ID Mem VCPUs State Time(s) Domain-0 0 256 2 r----- 14.2 DomD 1 1023 4 -b---- 23.3 root@generic-armv8-xt-dom0:~#
- Create a domain from config file <filename> (xl create <config file>)
root@generic-armv8-xt-dom0:~# xl list Name ID Mem VCPUs State Time(s) Domain-0 0 256 2 r----- 14.2 DomD 1 1023 4 -b---- 23.3 root@generic-armv8-xt-dom0:~# root@generic-armv8-xt-dom0:~# xl create /etc/xen/domu.cfg Parsing config from /etc/xen/domu.cfg libxl: info: libxl_create.c:121:libxl__domain_build_info_setdefault: qemu-xen is unavailable, using qemu-xen-traditional instead: No such file or directory (XEN) GICv3: Mapping ITS translation register to d3:addr=0x00000000f1050000 size=0x0000000000010000 libxl: error: libxl_arm.c:1137:copy_partial_fdt: Can't copy the node "/passthrough" from the partial FDT (XEN) memory_map:add: dom3 gfn=e6260 mfn=e6260 nr=10 (XEN) memory_map:add: dom3 gfn=37fc9 mfn=47fc9 nr=2 (XEN) ipmmu: /soc/iommu@eefc0000: d3: Set IPMMU context 3 (pgd 0x4f65a0000) (XEN) ipmmu: /soc/rswitch_osid1: Using IPMMU context 3 root@generic-armv8-xt-dom0:~# (XEN) d3v0: vGICD: RAZ on reserved register offset 0x00000c (XEN) d3v0: vGICD: unhandled word write 0x000000ffffffff to ICACTIVER4 (XEN) d3v0: vGICD: unhandled word write 0x000000ffffffff to ICACTIVER8 (XEN) d3v0: vGICD: unhandled word write 0x000000ffffffff to ICACTIVER12 (XEN) d3v0: vGICD: unhandled word write 0x000000ffffffff to ICACTIVER16 (XEN) d3v0: vGICD: unhandled word write 0x000000ffffffff to ICACTIVER20 (XEN) d3v0: vGICD: unhandled word write 0x000000ffffffff to ICACTIVER24 (XEN) d3v0: vGICD: unhandled word write 0x000000ffffffff to ICACTIVER28 (XEN) d3v0: vGICD: unhandled word write 0x000000ffffffff to ICACTIVER32 (XEN) d3v0: vGICD: unhandled word write 0x000000ffffffff to ICACTIVER36 (XEN) d3v0: vGICD: unhandled word write 0x000000ffffffff to ICACTIVER40 (XEN) d3v0: vGICD: unhandled word write 0x000000ffffffff to ICACTIVER44 (XEN) d3v0: vGICR: SGI: unhandled word write 0x000000ffffffff to ICACTIVER0 (XEN) d3v1: vGICR: SGI: unhandled word write 0x000000ffffffff to ICACTIVER0 (XEN) grant_table.c:1879:d3v1 Expanding d3 grant table from 1 to 2 frames (XEN) grant_table.c:1879:d3v1 Expanding d3 grant table from 2 to 3 frames root@generic-armv8-xt-dom0:~# xl list Name ID Mem VCPUs State Time(s) Domain-0 0 256 2 r----- 15.9 DomD 1 1021 4 -b---- 26.5 DomU 3 511 2 -b---- 7.5 root@generic-armv8-xt-dom0:~#
- Attach to domain's console (xl console DomD)
root@generic-armv8-xt-dom0:~# xl list Name ID Mem VCPUs State Time(s) Domain-0 0 256 2 r----- 15.9 DomD 1 1021 4 -b---- 26.5 DomU 3 511 2 -b---- 7.5 root@generic-armv8-xt-dom0:~# root@generic-armv8-xt-dom0:~# xl console DomD [ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x412fd050] [ 0.000000] Linux version 5.10.41-yocto-standard (oe-user@oe-host) (aarch64-poky-linux-gcc (GCC) 9.3.0, GNU ld (GNU Binutils) 2.34.0.20200220) #1 SMP PREEMPT Thu Jul 15 12:11:21 UTC 2021 [ 0.000000] Machine model: XENVM-4.17 [ 0.000000] Xen 4.17 support found (snip) s4sk-domd login: root root@s4sk-domd:~#
- Back to Dom0 : ctrl + ]
root@s4sk-domd:~# root@generic-armv8-xt-dom0:~# root@generic-armv8-xt-dom0:~#
- Attach to domain's console (xl console DomU)
root@generic-armv8-xt-dom0:~# xl list Name ID Mem VCPUs State Time(s) Domain-0 0 256 2 r----- 21.6 DomD 1 1021 4 -b---- 33.3 DomU 3 511 2 -b---- 8.2 root@generic-armv8-xt-dom0:~# xl console DomU [ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x412fd050] [ 0.000000] Linux version 5.10.41-yocto-standard (oe-user@oe-host) (aarch64-poky-linux-gcc (GCC) 9.3.0, GNU ld (GNU Binutils) 2.34.0.20200220) #1 SMP PREEMPT Thu Jul 15 12:11:21 UTC 2021 [ 0.000000] Machine model: XENVM-4.17 [ 0.000000] Xen 4.17 support found (snip) s4sk-domu login: root root@s4sk-domu:~#
- Back to Dom0 : ctrl + ]
- List the VCPUs for all/some domains (xl vcpu-list)
root@generic-armv8-xt-dom0:~# xl vcpu-list Name ID VCPU CPU State Time(s) Affinity (Hard / Soft) Domain-0 0 0 6 r-- 12.0 all / all Domain-0 0 1 1 -b- 11.4 all / all DomD 1 0 2 -b- 10.3 all / all DomD 1 1 3 -b- 7.9 all / all DomD 1 2 4 -b- 7.9 all / all DomD 1 3 5 -b- 9.2 all / all DomU 3 0 7 -b- 4.3 all / all DomU 3 1 0 -b- 4.2 all / all root@generic-armv8-xt-dom0:~#
- Set which CPUs a VCPU can use (xl vcpu-pin <domain ID> <vCPU> <physical CPUs>)
root@generic-armv8-xt-dom0:~# xl vcpu-list Name ID VCPU CPU State Time(s) Affinity (Hard / Soft) Domain-0 0 0 6 r-- 13.3 all / all Domain-0 0 1 1 -b- 12.6 all / all DomD 1 0 2 -b- 10.6 all / all DomD 1 1 3 -b- 8.9 all / all DomD 1 2 4 -b- 8.6 all / all DomD 1 3 5 -b- 10.3 all / all DomU 3 0 7 -b- 4.5 all / all DomU 3 1 0 -b- 4.3 all / all root@generic-armv8-xt-dom0:~# xl vcpu-pin 1 1 7 root@generic-armv8-xt-dom0:~# xl vcpu-list Name ID VCPU CPU State Time(s) Affinity (Hard / Soft) Domain-0 0 0 6 r-- 13.4 all / all Domain-0 0 1 1 -b- 12.7 all / all DomD 1 0 2 -b- 10.6 all / all DomD 1 1 7 -b- 8.9 7 / all DomD 1 2 4 -b- 8.6 all / all DomD 1 3 5 -b- 10.4 all / all DomU 3 0 7 -b- 4.5 all / all DomU 3 1 0 -b- 4.3 all / all root@generic-armv8-xt-dom0:~#
- Create multiple domains (xl create)
root@generic-armv8-xt-dom0:~# xl vcpu-list Name ID VCPU CPU State Time(s) Affinity (Hard / Soft) Domain-0 0 0 0 -b- 6.0 all / all Domain-0 0 1 1 r-- 4.4 all / all DomD 1 0 2 -b- 4.7 all / all DomD 1 1 3 -b- 4.1 all / all DomD 1 2 4 -b- 6.5 all / all DomD 1 3 5 -b- 3.3 all / all DomU 2 0 6 -b- 3.8 all / all DomU 2 1 7 -b- 3.8 all / all root@generic-armv8-xt-dom0:~# xl destroy DomU root@generic-armv8-xt-dom0:~# xl vcpu-list Name ID VCPU CPU State Time(s) Affinity (Hard / Soft) Domain-0 0 0 0 r-- 6.5 all / all Domain-0 0 1 1 -b- 4.7 all / all DomD 1 0 2 -b- 4.9 all / all DomD 1 1 3 -b- 4.4 all / all DomD 1 2 4 -b- 6.7 all / all DomD 1 3 5 -b- 3.5 all / all root@generic-armv8-xt-dom0:~# cp /etc/xen/domu.cfg /etc/xen/domu1.cfg root@generic-armv8-xt-dom0:~# cp /etc/xen/domu.cfg /etc/xen/domu2.cfg root@generic-armv8-xt-dom0:~# cp /etc/xen/domu.cfg /etc/xen/domu3.cfg root@generic-armv8-xt-dom0:~# vi /etc/xen/domu1.cfg Before: vif = [ 'backend=DomD, bridge=xenbr0, mac=08:00:27:ff:cb:cf' ] After : vif = [ 'backend=DomD, bridge=xenbr0, mac=08:00:27:ff:cb:d1' ] root@generic-armv8-xt-dom0:~# vi /etc/xen/domu2.cfg Before: vif = [ 'backend=DomD, bridge=xenbr0, mac=08:00:27:ff:cb:cf' ] After : vif = [ 'backend=DomD, bridge=xenbr0, mac=08:00:27:ff:cb:d2' ] root@generic-armv8-xt-dom0:~# vi /etc/xen/domu3.cfg Before: vif = [ 'backend=DomD, bridge=xenbr0, mac=08:00:27:ff:cb:cf' ] After : vif = [ 'backend=DomD, bridge=xenbr0, mac=08:00:27:ff:cb:d3' ] root@generic-armv8-xt-dom0:~# root@generic-armv8-xt-dom0:~# xl create /etc/xen/domu1.cfg 'name="DomU-1" ; vcpus="1" ; cpus="all" ; memory="128" ; tee = [] ; dt_passthrough_nodes = [] ; dtdev = [] ; irqs = [] ; iomem = [] ; renesas_vmq = []' Parsing config from /etc/xen/domu1.cfg libxl: info: libxl_create.c:121:libxl__domain_build_info_setdefault: qemu-xen is unavailable, using qemu-xen-traditional instead: No such file or directory (XEN) GICv3: Mapping ITS translation register to d3:addr=0x00000000f1050000 size=0x0000000000010000 root@generic-armv8-xt-dom0:~# (XEN) d3v0: vGICD: RAZ on reserved register offset 0x00000c (XEN) d3v0: vGICR: SGI: unhandled word write 0x000000ffffffff to ICACTIVER0 (XEN) grant_table.c:1879:d3v0 Expanding d3 grant table from 1 to 2 frames root@generic-armv8-xt-dom0:~# xl create /etc/xen/domu2.cfg 'name="DomU-2" ; vcpus="1" ; cpus="all" ; memory="128" ; tee = [] ; dt_passthrough_nodes = [] ; dtdev = [] ; irqs = [] ; iomem = [] ; renesas_vmq = []' Parsing config from /etc/xen/domu2.cfg libxl: info: libxl_create.c:121:libxl__domain_build_info_setdefault: qemu-xen is unavailable, using qemu-xen-traditional instead: No such file or directory (XEN) GICv3: Mapping ITS translation register to d4:addr=0x00000000f1050000 size=0x0000000000010000 root@generic-armv8-xt-dom0:~# (XEN) d4v0: vGICD: RAZ on reserved register offset 0x00000c (XEN) d4v0: vGICR: SGI: unhandled word write 0x000000ffffffff to ICACTIVER0 (XEN) grant_table.c:1879:d4v0 Expanding d4 grant table from 1 to 2 frames root@generic-armv8-xt-dom0:~# xl create /etc/xen/domu3.cfg 'name="DomU-3" ; vcpus="1" ; cpus="all" ; memory="128" ; tee = [] ; dt_passthrough_nodes = [] ; dtdev = [] ; irqs = [] ; iomem = [] ; renesas_vmq = []' Parsing config from /etc/xen/domu3.cfg libxl: info: libxl_create.c:121:libxl__domain_build_info_setdefault: qemu-xen is unavailable, using qemu-xen-traditional instead: No such file or directory (XEN) GICv3: Mapping ITS translation register to d5:addr=0x00000000f1050000 size=0x0000000000010000 root@generic-armv8-xt-dom0:~# (XEN) d5v0: vGICD: RAZ on reserved register offset 0x00000c (XEN) d5v0: vGICR: SGI: unhandled word write 0x000000ffffffff to ICACTIVER0 (XEN) grant_table.c:1879:d5v0 Expanding d5 grant table from 1 to 2 frames root@generic-armv8-xt-dom0:~# root@generic-armv8-xt-dom0:~# xl vcpu-list Name ID VCPU CPU State Time(s) Affinity (Hard / Soft) Domain-0 0 0 0 r-- 6.9 all / all Domain-0 0 1 3 -b- 7.2 all / all DomD 1 0 4 -b- 7.8 all / all DomD 1 1 6 -b- 5.6 all / all DomD 1 2 7 -b- 7.8 all / all DomD 1 3 5 -b- 5.1 all / all DomU 2 0 1 -b- 4.2 all / all DomU 2 1 2 -b- 3.8 all / all DomU-1 3 0 0 -b- 6.7 all / all DomU-2 4 0 2 -b- 7.1 all / all DomU-3 5 0 6 -b- 6.7 all / all root@generic-armv8-xt-dom0:~#
DomD
- Attach to domain's console (xl console DomD)
root@generic-armv8-xt-dom0:~# xl console DomD [ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x412fd050] [ 0.000000] Linux version 5.10.41-yocto-standard (oe-user@oe-host) (aarch64-poky-linux-gcc (GCC) 9.3.0, GNU ld (GNU Binutils) 2.34.0.20200220) #1 SMP PREEMPT Thu Jul 15 12:11:21 UTC 2021 (snip) s4sk-domd login: root root@s4sk-domd:~#
- Ethernet TSN
- S4SK TSN0(IC101) <-- LAN Cable --> PC
root@generic-armv8-xt-dom0:~# xl console DomD (snip) root@s4sk-domd:~# root@s4sk-domd:~# ifconfig tsn0 192.168.10.10 [ 1687.829480] rswitch_get_phy_node PHY interface = sgmii [ 1687.831104] libphy: rswitch_mii: probed [ 1687.879559] mv88x2110 etha0:01: Firmware version 8.5.0.0 [ 1687.915572] mv88x2110 etha0:01: attached PHY driver [mv88x2110] (mii_bus:phy_addr=etha0:01, irq=POLL) root@s4sk-domd:~# [ 1691.032980] renesas_eth_sw e68c0000.ethernet tsn0: Link is Up - 1Gbps/Full - flow control off [ 1691.033147] IPv6: ADDRCONF(NETDEV_CHANGE): tsn0: link becomes ready root@s4sk-domd:~# root@s4sk-domd:~# ifconfig tsn0 tsn0 Link encap:Ethernet HWaddr 74:90:50:D0:7B:58 inet addr:192.168.10.10 Bcast:192.168.10.255 Mask:255.255.255.0 inet6 addr: fe80::7690:50ff:fed0:7b58/64 Scope:Link UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1 RX packets:60 errors:0 dropped:3 overruns:0 frame:0 TX packets:17 errors:0 dropped:0 overruns:0 carrier:0 collisions:0 txqueuelen:1000 RX bytes:6835 (6.6 KiB) TX bytes:1380 (1.3 KiB) root@s4sk-domd:~# ping 192.168.10.116 PING 192.168.10.116 (192.168.10.116): 56 data bytes 64 bytes from 192.168.10.116: seq=0 ttl=127 time=1.123 ms 64 bytes from 192.168.10.116: seq=1 ttl=127 time=1.631 ms 64 bytes from 192.168.10.116: seq=2 ttl=127 time=1.009 ms root@s4sk-domd:~# root@s4sk-domd:~# ifconfig tsn1 192.168.11.11 root@s4sk-domd:~# ifconfig tsn1 tsn1 Link encap:Ethernet HWaddr E6:22:98:08:D9:C9 inet addr:192.168.11.11 Bcast:192.168.11.255 Mask:255.255.255.0 UP BROADCAST MULTICAST MTU:1500 Metric:1 RX packets:0 errors:0 dropped:0 overruns:0 frame:0 TX packets:0 errors:0 dropped:0 overruns:0 carrier:0 collisions:0 txqueuelen:1000 RX bytes:0 (0.0 B) TX bytes:0 (0.0 B) root@s4sk-domd:~#
- UFS
root@s4sk-domd:~# mount /dev/sda1 /mnt/ [ 869.252821] EXT4-fs (sda1): recovery complete [ 869.253400] EXT4-fs (sda1): mounted filesystem with ordered data mode. Opts: (null) root@s4sk-domd:~#
- * Click here to see how to format.
- Micro SD (CN5)
root@s4sk-domd:~# dmesg |grep mmcblk [ 0.000000] Kernel command line: root=/dev/mmcblk0p2 rw rootwait console=hvc0 clk_ignore_unused pci=pcie_bus_perf [ 3.646050] Waiting for root device /dev/mmcblk0p2... [ 3.829567] mmcblk0: mmc0:aaaa SC32G 29.7 GiB [ 3.833074] mmcblk0: p1 p2 p3 [ 4.145066] EXT4-fs (mmcblk0p2): recovery complete [ 4.148809] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null) [ 5.281648] EXT4-fs (mmcblk0p2): re-mounted. Opts: (null) root@s4sk-domd:~#
- Back to Dom0 : ctrl + ]
root@s4sk-domd:~# root@generic-armv8-xt-dom0:~# root@generic-armv8-xt-dom0:~#
DomU
- Attach to domain's console (xl console DomU)
root@generic-armv8-xt-dom0:~# xl console DomU [ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x412fd050] [ 0.000000] Linux version 5.10.41-yocto-standard (oe-user@oe-host) (aarch64-poky-linux-gcc (GCC) 9.3.0, GNU ld (GNU Binutils) 2.34.0.20200220) #1 SMP PREEMPT Thu Jul 15 12:11:21 UTC 2021 (snip) s4sk-domu login: root root@s4sk-domu:~#
- Back to Dom0 : ctrl + ]
root@s4sk-domd:~# root@generic-armv8-xt-dom0:~# root@generic-armv8-xt-dom0:~#
Known issues & Restrictions
Q&A site
If you have any questions, feel free to post them here.
https://community.renesas.com/automotive/gateway/
FAQ site
- https://en-support.renesas.com/knowledgeBase/category/31891 (English page)
- https://ja-support.renesas.com/knowledgeBase/category/31892 (Japanese page)