The E10A-USB emulator is an on-chip debugging emulator which supports the development for systems using microcomputers of the SuperH RISC engine family, the H8SX family, and the H8S family. As the main body of the E10A-USB emulator is connected to the user system via the dedicated debug interface (H-UDI and AUD), you can debug in such a form close to the completed product.

Features

  • Breakpoints
    • Hardware Breakpoints, dependent on device specification
    • 255 software breakpoints
    • User break
  • Trace functions
    • 4 branch trace messages stored on device H-UDI capable devices
    • Real time branch trace with AUD capable devices -HS0005KCU02H only
  • RAM monitor
    • The contents of a memory can be referenced and changed during program execution in real-time with AUD capable devices.
  • Full source level debug
    • Support for Renesas , IAR and GNU compilers
  • Host requirement
    • PentiumR3 600MHz or greater
    • RAM 128MB or greater
    • Available hard-disk 50MB or greater
    • USB rev 1.1 port
  • User I/F
    • 14-way connector (Type: 2514-6002: [3M Co., Ltd.])
    • 36-way connector (Type: DX10M-36S: [Hirose Electric Co., Ltd.])
  • Learn More

Documentation & Downloads

Title language Type Format File Size Date
User Guides & Manuals
On-chip Debuggers Performance Property 日本語 Manual PDF 213 KB
Technical Updates
Problem with the E10A-USB Emulator while Using the SH7290 日本語 Technical Update PDF 21 KB
Limitation due to a conflict between the refresh controller and break interrupts 日本語 Technical Update PDF 21 KB
Limitation on operation of the watchdog timer (WDT) due to a problem with the library for programming and erasing data in the flash memory (TN-EML-A123A/E) 日本語 Technical Update PDF 25 KB
Limitation on Handling the [IO] Window Due to a Problem with the Device 日本語 Technical Update PDF 21 KB
Downloads
High-performance Embedded Workshop V.4.09.01 Full Update 日本語 Upgrade - IDE EXE 68.25 MB
High-performance Embedded Workshop V.4.09.01 Differential Update(From V.4.09.00) 日本語 Upgrade - IDE EXE 15.89 MB
Renesas E-Series USB Driver V.1.02 Release 00 日本語 Upgrade - IDE EXE 3.25 MB
High-performance Embedded Workshop V.4.05.01 Full Update Upgrade - IDE EXE 58.81 MB
High-performance Embedded Workshop V.4.05.01 Differential Update(From V.4.05.00) Upgrade - IDE EXE 8.78 MB
Flash Memory Download Program for E10A-USB Emulator (For flash memory at word mode by Fujitsu Inc.) Sample Code 日本語 Sample Code ZIP 25 KB
Flash Memory Download Program for E10A-USB Emulator (For flash memory at byte mode by Renesas Electronics) Sample Code 日本語 Sample Code ZIP 15 KB
Flash Memory Download Program for E10A-USB Emulator (For flash memory at byte mode by Intel®) Sample Code 日本語 Sample Code ZIP 15 KB
Flash Memory Download Program for E10A-USB Emulator (For flash memory at word mode by Renesas Electronics) Sample Code 日本語 Sample Code ZIP 14 KB
Flash Memory Download Program for E10A-USB Emulator (For flash memory at word mode by Intel®) Sample Code 日本語 Sample Code ZIP 14 KB
Tool News
[Notes] E10A-USB Emulators HS0005KCU01H and HS0005KCU02H 日本語 Tool News - Note PDF 86 KB
A Note on Using the Licensed Tools for Adding Device Groups to E10A-USB Emulators' Support Lines 日本語 Tool News - Note PDF 196 KB
The E10A-USB On-Chip Debugging Emulator for the SH7205 and SH7265 MCU Groups --HS0005KCU04H--Released 日本語 Tool News - Release PDF 195 KB
A Note on Using the E10A-USB and E200F Emulator Software 日本語 Tool News - Note PDF 196 KB
A Note on Using the Emulator Software Packages for the E10A-USB Emulators and an E200F Emulator 日本語 Tool News - Note PDF 196 KB
A Note on Using the Emulator Software Packages for the E10A-USB, E10A, E200F, and E10T Emulators 日本語 Tool News - Note PDF 195 KB
A Note on Using the E200F and E10A-USB Emulators for the SH-2A-Cored MCUs 日本語 Tool News - Note PDF 197 KB
Notes on Using the E200F and E10A-USB Emulator Software Packages 日本語 Tool News - Note PDF 196 KB
A Note on Using the E10A-USB and E10A Emulators 日本語 Tool News - Note PDF 193 KB
A Note on Using the E200F and E10A-USB Emulators for the SH-2A Series of MCUs 日本語 Tool News - Note PDF 194 KB

Lineup

See the product pages for the details of each model below.

Item Description
Products HS0005KCU01H
for the H-UDI interface Note1
Image
E10AUSB-hs0005kcu01h
HS0005KCU02H
for the AUD trace function Note2 
Image
E10AUSB-hs0005kcu02h
HS0005KCU14H
for the Multi-core MCUs of SuperH RISC engine Family
Image
E10AUSB-hs0005kcu14h
MCUs
  • ・SuperH RISC engine Family (Excepting for the multi-core MCUs.)
  • ・H8SX Family
  • ・H8S Family
・Multi-core MCUs of SuperH RISC engine Family

Notes

  1. The H-UDI (User Debugging Interface) is an interface compatible with the Joint Test Action Group (JTAG) specifications.
  2. The AUD (Advanced User Debugger) trace is the large-capacity trace function that is enabled when the AUD pins are connected to the emulator. When an event that starts trace acquisition occurs, the trace information is output in realtime from the AUD pins. For more details, refer to On-chip Debuggers Performance Property (PDF | English, 日本語).