Open, Scalable Platform with 60 TOPS of Deep Learning Performance, Low Power, and Air Cooling System Drives Central Processing ECUs for Automated Driving

December 17, 2020

TOKYO, Japan ― Today, Renesas Electronics Corporation (TSE:6723), a premier supplier of advanced semiconductor solutions, unveiled the R-Car V3U – a best-in-class ASIL D system on chip (SoC) for advanced driver assistance systems (ADAS) and automated driving (AD) systems. Delivering a groundbreaking 60 TOPS with low power consumption for deep learning processing and up to 96,000 DMIPS, the R-Car V3U is built for the performance, safety, and scalability (up and down) demands of ADAS and AD architectures driving next-generation autonomous vehicles.

The new R-Car V3U is the first SoC using the R-Car Gen 4 architecture within the open and flexible Renesas autonomy platform for ADAS and AD. With the launch of R-Car V3U, the platform is now ready to offer complete scalability from entry-level NCAP applications up to highly automated driving systems.

“We are excited to introduce the newest generation of our popular R-Car SoCs for the next generation of ADAS and AD vehicles,” said Naoki Yoshida, Vice President, Automotive Digital Products Marketing Division at Renesas. “The R-Car V3U leverages assets developed on previous-generation devices, such as ADAS and Level 2 perception stack with the R-Car V3M and R-Car V3H, along with the Renesas autonomy platform, to offer a smooth migration path to single-chip Level 3 automated driving with short development turnaround and safe production launch.”

Best-in-class SoC to support the industry’s stringent ASIL D requirements:

Automated driving systems require functional safety up to ASIL D – the highest and most stringent automotive safety integrity level specified under the ISO 26262 standard for road vehicles. The best-in-class R-Car V3U SoC integrates multiple sophisticated safety mechanisms that provide high coverage with fast detection and response for random hardware faults, and is expected to achieve ASIL D metrics for the majority of the SoC processing chain, as well as reducing design complexity, time to market, and system cost.

State-of-the-art R-Car deep learning technology at low power consumption

The R-Car V3U delivers highly flexible DNN (Deep Neural Network) and AI machine learning functions. Its flexible architecture is capable of handling any state-of-the-art neural networks for automotive obstacle detection and classification tasks while maintaining 60 TOPS with low power consumption and an air cooling system.

The R-Car V3U also offers a wide range of programmable engines, including DSP for radar processing, multi-threading computer vision engine for traditional computer vision algorithms, image signal processing to enhance image quality, and additional hardware accelerators for key algorithms such as dense optical flow, stereo disparity, and object classification.

Sophisticated embedded software platform development for automated driving

Renesas has developed an open and integrated development environment that enables customers to take advantage of the R-Car platform’s built-in hardware benefits, as well as low power consumption and deterministic real-time software to enable fast time to market for computer vision and deep learning-based solutions.

Easy-to-use debugging and tuning tools for heterogeneous multi-core hardware enable efficient software development while a comprehensive set of example applications and online education resources allows engineers at all levels to jumpstart their design process. Qualified compilers and code generators for compliance with functional safety and cyber security requirements enable the development of safe and secure software development.

Customers can also combine the R-Car V3U with Renesas’ high-performance, low-power RH850 microcontroller, integrated power management ICs, and power transistor devices to access all the key components required for their ADAS and AD ECUs. This combination also enables them to efficiently develop their systems and speed their time to market.

Availability

Samples of the R-Car V3U SoC are available now. Mass production is planned for second quarter of 2023. For more information, please visit: renesas.com/r-car-V3U

Note 1: Deep neural networks (DNNs), are deep, feed-forward artificial neural networks that have been successfully applied for analyzing visual imagery and are increasingly used in automotive for applications like road detection or object classification.

About Renesas Electronics Corporation

Renesas Electronics Corporation (TSE: 6723) delivers trusted embedded design innovation with complete semiconductor solutions that enable billions of connected, intelligent devices to enhance the way people work and live. A global leader in microcontrollers, analog, power, and SoC products, Renesas provides comprehensive solutions for a broad range of automotive, industrial, infrastructure, and IoT applications that help shape a limitless future. Learn more at renesas.com. Follow us on LinkedIn, Facebook, Twitter, and YouTube.

(Remarks). All names of products or services mentioned in this press release are trademarks or registered trademarks of their respective owners.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.

Share this news on