With Broad Market Applications, the Robust IDT® ZMID520x Sensors Eliminate the Issue of Magnetic Stray Fields and Deliver Application Flexibility and a Reduced Bill of Material

March 27, 2017

SAN JOSE, Calif., March 27, 2017—Integrated Device Technology, Inc. (IDT) (NASDAQ: IDTI) today introduced a new family of high-performance inductive position sensors offering superior reliability, flexibility and serviceability while cutting system costs. The three ZMID520x sensors are automotive qualified to the AEC-Q100 standard and support implementation in safety-related systems compliant to ISO26262 up to ASIL-B.

The new sensors are ideal for the automotive, industrial and consumer markets and can be used for such end products as vehicles, robots, home appliances and smart automation.

By utilizing an inexpensive printed circuit coil and a simple metallic target, the ZMID520x sensors do away with magnets commonly used with position sensors, offering higher reliability and lowering costs. And, IDT’s inductive technology is immune to magnetic stray fields--parasitic magnetic fields that can cause electro-magnetic interference (EMI) and introduce safety risks. No expensive and complex shielding is required.

“The ZMID520x family represents a new, smarter approach to position sensing,” said Mario Montana, vice president and general manager, IDT’s Automotive and Industrial Products Division. “We have eliminated the need for a magnet—as well as the headache of magnetic stray fields—to boost reliability and hold down system costs.”   

The adaptable mechanical design enables rotational end-of-shaft, side-shaft, linear and arc motion, from small angles up to full 360°. The scalable coil design is tolerant to mechanical misalignment in any direction, horizontal or vertical. The sensor ICs can withstand ambient temperatures up to +150°C as well as other harsh conditions such as dust or humidity. Further, the coils themselves can be subjected to even more severe conditions, such as temperatures higher than 150°C as well as corrosive liquids or gases. Using only three wires, the sensor ICs can be user programmed and calibrated in the final system assembly without requiring additional wiring or components.

The three ZMID520x sensors provide a variety of outputs: the ZMID5201 for analog, the ZMID5202 for pulse-width modulation (PWM), and the ZMID5203 for the SENT (single edge nibble transmission) protocol. Learn more about the ZMID520x family in this video.

About IDT

Integrated Device Technology, Inc. develops system-level solutions that optimize its customers’ applications. IDT’s market-leading products in RF, real-time interconnect, wireless power transfer, serial switching, interfaces, automotive ASICs, battery management ICs, sensor signal conditioner ICs and environmental sensors are among the company’s broad array of complete mixed-signal solutions for the communications, computing, consumer, automotive and industrial segments. Headquartered in San Jose, Calif., IDT has design, manufacturing, sales facilities and distribution partners throughout the world. IDT stock is traded on the NASDAQ Global Select Stock Market® under the symbol “IDTI.” Additional information about IDT can be found at www.IDT.com. Follow IDT on Facebook, LinkedIn, Twitter, YouTube and Google+.

###

© 2017, IDT. IDT and the IDT logo are trademarks or registered trademarks of Integrated Device Technology, Inc. or its wholly-owned subsidiaries around the world. All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners.

Share this news on