May 8, 2015

TOKYO, Japan, May 8, 2015 — Renesas Electronics Corporation (TSE: 6723), a premier provider of advanced semiconductor solutions, today announced a new wireless solution that supports the Bluetooth® Smart near field wireless communication standard. The new RL78/G1D Group of microcontrollers (MCUs) has been developed by combining the low-power RF Transceiver Technology for Bluetooth® Low Energy (BLE), which the company presented at the International Solid-State Circuits Conference (ISSCC) held in February, 2015, with Renesas’ expertise on consumer and industrial MCUs, and on-chip peripheral devices necessary for wireless communication. By employing an evaluation kit and Bluetooth-SIG qualified protocol stack, the new MCUs enable system designers to conduct evaluation of wireless characteristics and initial evaluation of communication behaviors. The new MCUs are also provided with PC GUI tool for easy manipulation of these components. These will enable customers to easily develop Bluetooth Smart applications and reduce the time required for development while making effective use of development environment and software resources.

BLE is a near field wireless communication technology that holds great potential for connecting smartphones and a variety of other devices. In addition to smartphones, it is also suitable for use in devices linked by serial communication technologies such as UARTs and for implementing communication between units within a single piece of equipment. Eliminating the need for wired connections between such units provides greater design freedom and simplifies maintenance. This technology therefore has the potential to bring about major changes in embedded devices.

The Bluetooth Smart compliant RL78/G1D MCUs have been developed by combining the ultra-low-power RL78 MCU, which has achieved widespread adoption in the consumer and industrial fields, with the highly regarded low-current-consumption Bluetooth® low energy transceiver technology announced at the ISSCC in February 2015.

The current consumption of the RL78/G1D is among the lowest in the industry (3.5 milliamperes (mA) during reception and 4.3 mA during transmission), delivering substantially reduced power consumption that is a key consideration for wireless devices. A newly added adaptable RF technology adjusts the power consumption during wireless operation to the optimal level to match the communication distance. This dramatically lowers the power consumption of near field wireless communication, and it is complemented by the on-chip integration of most elements required for the antenna connection, contributing to reduced external component costs.

Key features of the new RL78/G1D MCUs:

(1) On-chip balun elements required for antenna connection simplify antenna connection circuit design

The new RL78/G1D integrates on-chip the balun elements that otherwise would have to be provided in an external antenna connection circuit. This makes it possible simply to connect the RF transceiver signal terminals to the external antenna terminals without the need for discrete balun elements. This eliminates the need to perform repeated matching adjustment and evaluation on a balun circuit, thereby saving on development costs. In addition, the components of the balun circuit do not have to be provided externally, lowering both the product cost and component management costs. Thus, production costs are reduced as well.

(2) Industry-leading low current consumption for extended battery life

The newly developed low-current-consumption on-chip RF transceiver supports version 4.1 of the Bluetooth Core Specification and enables wireless operation at among the lowest power consumption levels in the industry (3.5 mA during reception and 4.3 mA during transmission, at 0 dBm). This, combined with the excellent power efficiency of the RL78 family of ultra-low-power MCUs, makes for extended battery life. For example, when wireless communication takes place at one-second intervals while maintaining a connected state with another wireless device, the BLE functionality can be added with the industry-leading low average current of 10 μA.

(3) Function that automatically optimizes power consumption during wireless operation to match communication conditions

Built-in adaptable RF functionality optimizes the power consumption during wireless operation to match the communication distance. This prevents more power than necessary from being used, especially during near field communication. By using this functionality, under communication conditions where the wireless devices are located approximately 1 meter apart (varies according to the connection status) and when the frequency of wireless operation are raised in order to prioritize data transfer, it is possible to boost power efficiency.

Renesas positions the new RL78/G1D as a product that contributes to the near field wireless communication market, which is expected to grow with the coming of a more energy-efficient “smart society” and IoT. Renesas intends to continue to respond to the needs of the market with a broad lineup of products designed for ease of use.

Renesas at ESEC

Renesas Electronics will showcase demonstrations featuring RL78/G1D MCUs at the 18th Embedded Systems Expo (ESEC) to be held at Tokyo Big Sight from May 13 to 15, 2015, as part of Japan IT Week.

Pricing and Availability

The new RL78/G1D Group comprises of six product versions - 256, 192 & 128 KB on-chip flash memory options and industrial or consumer grade for each memory option. Samples are available now. Pricing varies depending on memory capacity. For example, the R5F11AGJ MCU with 256 KB of flash memory equipped on WQFN package with 48 pins is priced at US$3 per unit in sample quantities of 10,000. Mass production is scheduled to begin in October 2015 and is expected to reach a combined volume of 1,000,000 units per month in 2016. (Pricing and availability are subject to change without notice.)

Refer to the separate sheet (PDF: 67 KB) for the main specifications of Renesas' new RL78/G1D MCUs.

For more product information, please visit: https://www.renesas.com/en/products/microcontrollers-microprocessors/rl78/rl78g1x/rl78g1d.html

About Renesas Electronics Corporation

Renesas Electronics Corporation (TSE: 6723) delivers trusted embedded design innovation with complete semiconductor solutions that enable billions of connected, intelligent devices to enhance the way people work and live. A global leader in microcontrollers, analog, power and SoC products, Renesas provides comprehensive solutions for a broad range of automotive, industrial, infrastructure, and IoT applications that help shape a limitless future. Learn more at renesas.com. Follow us on LinkedIn, Facebook, Twitter, and YouTube.

(Remarks) Bluetooth® is a registered trademark of Bluetooth SIG, Inc. of the United States. All names of products or services mentioned in this press release are trademarks or registered trademarks of their respective owners.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.

Share this news on