Combines All Functions Needed for Wireless Charging on a Single Chip to Enable Compact Devices Resistant to Water and Dust

September 26, 2016

TOKYO, Japan, September 26, 2016 — Renesas Electronics Corporation (TSE: 6723), a premier supplier of advanced semiconductor solutions, today announced a contactless wireless charging solution for low-power applications, such as hearing aids and other wearable devices. that require resistance to water and dust.

The new wireless charging solution consists of a power receiver integrated circuit (IC) (RAA457100) and a power transmitter IC (RAA458100). Each IC includes all functions needed for wireless charging on a single chip. Renesas will also offer an evaluation kit to help manufacturers with their wireless charging designs.

Wireless charging technology eliminates the need to change batteries or connect a power cable. This convenience has wide appeal for a variety of applications, such as smartphones and wearable devices. Wireless charging technology is of particular interest in low-power applications such as hearing aids that require small form factors as well as resistance to water and dust. However, existing wireless charging technologies have been considered unsuitable for charging systems employing compact lithium-ion (Li-ion) secondary batteries for these low-power applications associated with the difficulties in; achieving smaller form factors with the antenna size mandated by the current standards; and heat dispersion due to large charging currents that are required to charge low-power applications.

With the new wireless charging solution, Renesas has combined its wireless charging system expertise with its proven microcontrollers (MCUs) to enable all key system components in a small space for easier design implementation.

Key features of the RAA457100 Power Receiver IC:

(1) Enabling more compact devices by integrating all functions needed for wireless charging in a 3.22mm x 2.77mm package

The power receiver IC incorporates a synchronous rectifier circuit that rectifies the AC power used to excite the antenna coil of the power receiver into direct current, and a charging control circuit for charging a lithium (Li-ion) secondary battery. A 12-bit A/D converter is used to monitor the battery voltage and current during charging, and this data is supplied to the power transmitter to maintain the optimal charging power level. Protection features for the Li-ion secondary battery and a DC/DC regulator are also incorporated on a single chip.

(2) On-chip DC/DC converter with industry-leading efficiency of 85 percent for extended operation on battery power

Low-power applications such as wearable devices and hearing aids generally use compact batteries with small capacities, making efficiency crucial. The integrated DC/DC converter itself achieves industry-leading high efficiency of 85 percent when the system is operating at a low load level of around 1 mA, which enables longer battery life.

Key features of the RAA458100 Power Transmitter IC:

(3) Integration of all circuits needed for wireless power transmission and support for single 5 V power supply voltage from mobile batteries

In general, contactless power transmission involves applying a 125 kHz alternating current to the antenna coil of the power transmitter to excite the antenna coil of the power receiver and generate AC power. Renesas’ newly developed power transmitter IC drives a bridge circuit and controls the alternating current to obtain the transmission power value required by the power receiver. The power transmitter IC integrates a bridge circuit overcurrent protection function and a two-line external overheating protection function. System manufacturers can modify parameter values by programming the read registers with external EEPROM data via an I2C interface to meet their application needs. In addition, they can further customize the solution to their requirements by connecting an external MCU.

The μPA2690T1R power MOSFET from Renesas is recommended for configuring the bridge circuit. When it is combined with the RAA458100, the system manufacturer can choose between half-bridge and full-bridge circuit configurations to match the power level of the power transmitter.

Availability

Samples of the new wireless charging system solution will be available in November 2016. (Availability is subject to change.)

Renesas is positioning the new solution as a solution for system manufactures to easily add wireless charging functionality to low-power applications such as wearable devices and hearing aids.

Please refer to the separate sheet (PDF: 110 KB) for the main specifications of the wireless charging system solution.

For more information on the wireless charging solution, please visit: https://www.renesas.com/en/promotions/products-solutions/wireless-charging.html

About Renesas Electronics Corporation

Renesas Electronics Corporation (TSE: 6723) delivers trusted embedded design innovation with complete semiconductor solutions that enable billions of connected, intelligent devices to enhance the way people work and live. A global leader in microcontrollers, analog, power, and SoC products, Renesas provides comprehensive solutions for a broad range of automotive, industrial, infrastructure, and IoT applications that help shape a limitless future. Learn more at renesas.com. Follow us on LinkedIn, Facebook, Twitter, and YouTube.

(Remarks) All registered trademarks or trademarks are the property of their respective owners.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.

Share this news on