Image
Minoru Uemura
Minoru Uemura
Principal Product Marketing Specialist
Published: July 11, 2023

First of all, Renesas would like to thank the many customers who use the RH850/F1x series.

Since the launch of the RH850/F1x series with the birth of Renesas Electronics, the company has shipped more than 1.6 billion units to the market and continues to renew the portfolio. Behind this is many evolutions that are close to the market, such as higher performance, larger memory, and diversification of packages.

Image
RH850 F1X Series Evolution F1L To F1KH

Recent years, there has been an increasing number of cases that legacy product design assets are evolved to respond to the evolution of E/E architecture in the automotive actuator ECU market, which is the main application of the RH850/F1x series.
The key point is to diversify the product lineup, such as "high performance with small memory and the same footprint" and "diversification of memory options".

To meet these market needs, we will expand customer options by adding the RH850/F1KM-S2 series, which covers the space between the RH850/F1K series and the RH850/F1KM-S4 series.

Image
Expand Customer Options by Adding the RH850 / F1KM-S2 series

Here, we will introduce two examples of the RH850/F1KM-S2.

#CASE1: Easily supports program size reduction

The user is using RH850/F1KM-S4 with OTA support during the development, a total of 4MB code flash is used, 2MB for application and 2MB for backup. The OTA requirement is removed for production so that only 2MB code flash is needed. In such a case, the RH850/F1KM-S2 enables development with minimal hardware and software changes.

Image
#CASE1: Easily supports program size reduction

#CASE2:  Easily respond to enhanced security demands

In a project under development on RH850/F1KM-S1, security requirements have been enhanced, and Evita-Mid support is required. Since the 1MB ROM space was exhausted, it was necessary to add security firmware and update the HSM (Hardware Security Module) to support Evita-Mid. In such a case, the RH850/F1KM-S2 enables development with minimal hardware and software changes.

Image
#CASE2: Easily respond to enhanced security demands

Renesas will continue to release products that will satisfy our customers, so please look forward to it.

For more information is available on the RH850 F1KM-S2 products page.
You can purchase both the device and development kits from the Renesas online store.

Share this news on