Overview

Description

Topics
RZ Smart Configurator supports the new device RZ/V2H group, Quad-core Vision AI MPU with DRP-AI3 Accelerator and High-Performance Real-time Processor.
[Upgrade to Revision] Smart Configurator for RZ V1.17.0 (PDF | English, 日本語)

RZ Smart Configurator automatically generates initial-setting programs for MCUs.
It provides a quick and smart way of combining and configuring software to meet your needs, such as by configuring peripheral pins and importing middleware and drivers.

*The installer format differs depending on the device. For details, refer to Release Information.

Features

  • Importing Middleware/Drivers
  • Pin Settings
  • Learn More

Release Information

MCUsSupported IDEsRelated documentsLatest Ver.
Released
Operating Environment
e² studioIARStand-alone
RZ/A2check
(Note1)
RZ/A2M Smart Configurator User Guide: e² studio (PDF | English, 日本語)
Details of the RZ/A2M Software Package
V7.8.0
Apr 20, 2020
Details of e² studio upgrade
Operating Environment
RZ/A3ULcheck
(Note2)
RZ/A Getting Started with Flexible Software Package (PDF)
Details of the RZ/A3UL Software Package
V2022-07
Details of e² studio upgrade
RZ/T2check
(Note3)
cloud_downloadRZ/T2,RZ/N2 Getting Started with Flexible Software Package (PDF)V2023-01
Details of e² studio upgrade
RZ/N2cloud_download
RZ/G2 (Sub CPU)(Note4)
RZ/V2L (Sub CPU)(Note5)
checkRZ/G2L and RZ/G2UL Group Multi-OS Package
RZ/V2L Group Multi-OS Package
V2022-07
Details of e² studio upgrade
RZ/A1, RZ/G1,
RZ/G2 (Main CPU), RZ/G3S, 
RZ/V2L (Main CPU),
RZ/V2H (Main CPU)
cloud_download
(Note6)
32-bit version: V1.10.1
Aug 05, 2021
Details of upgrade
cloud_download 64-bit version:(Note7) V1.17.0
Mar 05, 2024
Details of upgrade

— : Not Supported

Note

  1. The package of the e² studio includes this plug-in.
  2. Installation RZ/A FSP Packs is mandatory.
    RZ/A FSP Packs >>
  3. Download platform installer or smart configurator included FSP (Flexible Software Package) from FSP web page of Renesas.
    RZ/T2 Platform Installer >>
    RZ/N2 Platform Installer >>
  4. Support RZ/G2 devices included Sub CPU. Support device Group: RZ/G2L、RZ/G2LC、RZ/G2UL
    For using these features of smart configurator, e² studio and ‘RZ/G2L and RZ/G2UL Group Multi-OS Package’ must be installed.
  5. For using these features of smart configurator, e² studio and ‘RZ/V2L Group Multi-OS Package’ must be installed.
  6. The Smart Configurator for the RZ/G groups only generates Device Tree Specification (DTS) include files (dtsi), which are only usable in the development environment of the Linux platform. Manually merge the device-setting code in the generated dtsi files with the default dtsi files included in your source code produced under Linux for an RZ/G device. For details of the DTS, refer to the links on https://www.devicetree.org/specifications/.
  7. Smart Configurator of RZ V1.11.0 and later will support the 64-bit versions of Windows® only.
End of Support for Windows 32-Bit Versions
Smart Configurator released after Dec. 2021 will support the 64-bit versions of Windows® only.
Microsoft® Windows® has shifted to the 64-bit environment. Therefore, Renesas will focus on supporting Smart Configurator for the 64-bit environment.
(Microsoft®, Windows® are registered trademarks of Microsoft Corporation in the United States and/or other countries. https://www.microsoft.com/legal/intellectualproperty/trademarks.aspx)

 

Target Devices

Note

  1. RZ/A1 series: Only the pin-assignment function is supported.
  2. RZ/G, V series: Only the pin-assignment function and the pin-setting code generation (DTS) function are supported.

Downloads

Type Title Date
Software & Tools - Software Log in to Download EXE 196.48 MB 日本語
1 item

Documentation

Smart Configurator Introduction

Smart Configurator (SC) is a GUI-based tool that can generate code for drivers and middlewares and configure pins easily.

  • Smart Configurator overview
  • Centralized resource management
  • Easy, Efficient, Expansion.

Additional Details

Pin Settings

The assignments of pins can be set up through a GUI, which also checks and offers solutions for cases of contention for the same pin by multiplexed functions.

The [Pins Configuration] window (displayed per peripheral module)

Image

Specifying a peripheral module in the [Pins Configuration] window displays the pin functions for use by the module and allows you to set the assignment of the functions to pins.

[MCU Package] window

Image

The [MCU Package] window displays a symbolic view of the pins, indicating by colors which pins are and are not in use, which have been assigned contending multiplexed functions, and so on. This makes it easy to check the overall situation.

Automatic resolution of contention between pin functions

Image

In cases of contention for a pin, clicking on the pin brings up a list allowing automatic changing of the assignment of the pin to resolve the contention.

Output a Device Settings File for Linux (Note1)

Output a DTS file that contains pin settings. You can readily apply device settings to Linux.

Note

  1. Only for the devices supported by the  Verified Linux Package (RZ/G1, RZ/G2, RZ/V2L)

 

Importing Middleware/Drivers

Flexible Software Package(FSP)(Note1)

Image

You can change the settings of FSP pins and components by using the Smart Configurator GUI.

Note

  1. Available only for the RZ Family devices supported by the FSP.

RZ/A2M Software Package (Note1)

The RZ/A2M Software Package consists of a range of middleware and drivers, which you can import and then modify settings such as pin assignments as required.
Details of the RZ/A2M Software Package >>

Note

  1. We currently support version 2.0.0 and later versions of the RZ/A2M Software Package.

 

Supported Features

MCUsFlexible Software Package supportImporting middlewareGenerating driver codePin settings
RZ/A1H   RZ/A1L   RZ/A1LU   RZ/A1M
RZ/Five
RZ/G1C   RZ/G1E   RZ/G1H   RZ/G1M   RZ/G1N
RZ/G2E   RZ/G2H   RZ/G2M  RZ/G2N 
RZ/G2L   RZ/G2LC  RZ/G2UL  
RZ/V2L   RZ/V2H
lens
RZ/A2Mlenslenslens
RZ/A3UL 
RZ/N2L   RZ/T2M   RZ/T2L
RZ/G2L (Sub CPU) (Note1) 
RZ/G2LC (Sub CPU)   RZ/G2UL (Sub CPU)
RZ/V2L (Sub CPU) (Note2)
lenslenslenslens

— : Not Supported

Note

  1. Support RZ/G2 devices included Sub CPU. Support device Group: RZ/G2L、RZ/G2LC、RZ/G2UL
    For using these features of smart configurator, e² studio and‘RZ/G2L and RZ/G2UL Group Multi-OS Package’must be installed.
  2. For using these features of smart configurator, e² studio and‘RZ/V2L Group Multi-OS Package’must be installed.