概览

简介

最佳化且紧密集成的适用软件套,具备可扩展最终产品复杂性并简化复杂系统级服务的商用RTOS。

特性

  • Synergy MCU具有强大的通用API
  • 用于抽取和代码再利用的应用程序框架
  • ThreadX®,一款经过验证的商业RTOS
  • X-Ware™、NetX Duo™、NetX Secure™、USBX™、GUIX™、FileX®
  • 灵活的分层式架构
  • 开发于IEC/ISO-12207软件生命周期过程
  • 可按SSP数据表所指定的内容运行

*Important Notice:
 On November 21, 2023, Microsoft announced that they have decided to contribute Azure RTOS to Open Source under the stewardship of the Eclipse foundation and Azure RTOS becomes Eclipse ThreadX.

For detailed information, please refer to the announcement titled at Microsoft Contributes Azure RTOS to Open Source.

The support strategy scheme for Eclipse ThreadX will be determined and communicated at a later date.

Microsoft will discontinue the Azure RTOS and Azure RTOS Middleware. It’s important to note that updates for Azure RTOS on this hardware will no longer be provided.

发布信息

SSP 2.6.0

Current Public Release

Release Date: 2024-03-29

MCUs Supported: S7G2, S3A7, S124, S3A3, S128, S5D9, S5D5, S5D3, S3A6, S3A1, S1JA

What's New?

SSP v2.6.0 is a minor release with new stack updates, enhancements, and quality improvements.

License Update

  • SSP 2.6.0 no longer requires license keys

Software Tools Updates

  • e2studio and SSC 2024-01.1
  • QE Tool for CTSU v3.3.0
  • CMSIS base v5.8.0, including CMSIS Core-M v5.5.0, CMSIS DSP v1.9.0, and CMSIS NN v3.0.0

Azure RTOS Stack Updates

  • ThreadX v6.2.1
  • USBX v6.2.1
  • FileX v6.2.1
  • GUIX v 6.2.1 and GUIX Studio v 6.2.1 or higher
  • TraceX v6.2.1 or higher
  • LevelX v6.2.1
  • NetX, NetX Duo and NetX Secure v6.2.1

Bug Fixes

Installation Instructions

Refer to the Release Notes for Installation instructions.

目标设备

下载

类型 文档标题 日期
软件和工具 - 软件 登录后下载 ZIP 1,729.62 MB
软件和工具 - 软件 登录后下载 ZIP 68.70 MB
软件和工具 - 软件 登录后下载 ZIP 737.49 MB
3 items

文档

SSP 术语表

SSP组件由瑞萨紧密集成、优化、测试、记录并维护。分层式架构使开发人员能够使用通用的API和应用程序框架来编写应用程序,或根据需要直接连接到设备驱动程序级别。此处可了解每个SSP组件的功能。

浏览 SSP 术语表

软件质量

Renesas has established a Software Quality Assurance (SQA) process for the SSP to cover the necessary Testing and Software Development Life Cycle (SDLC).

SSP quality is tracked and measured using combinations of unit, functional, integration, performance, regression, dynamic, and static analysis tests. To ensure high quality, production grade Software, SSP is developed and tested to ensure adherence with the four quality metrices

  • 符合编码标准
  • 保持低代码复杂性有跟踪要求
  • 便于创建
  • 全面的模块和系统级测试

Get information about open source software included in SSP.

 

Synergy™独立配置器(SSC)

SSC是一款Eclipse富客户端平台应用程序,它可以在e2 studio ISDE中复制Synergy项目生成器和项目编辑器工具的功能,从而为用于Renesas Synergy™的IAR Embedded Workbench®用户提供图形组件配置。

Synergy项目生成器提供引导式设置流程,其中包含选择设备、调试器和编译器选项。生成的预配置项目含有必要支持文件(如特定于设备的标题),可随时用于构建和调试。

利用Synergy项目编辑器,用户可以设置时钟树并配置I/O引脚。它包含Synergy软件包(SSP)模块配置器,可将SSP模块添加至各个RTOS线程、消息传递框架设置和中断启用。

下图显示了用于Renesas Synergy™的IAR Embedded Workbench®、SSC和SSP如何一起运行以创建Synergy项目。

 

IAR EW for Synergy