The M32100T-EZ-E is an emulator which has various debugging functions supporting M32R Family MCUs, including those with high-speed operation. Each M32R device includes one from a series of JTAG-based debugging interfaces called SDI (Scalable Debug Interface), and this emulator allows on-chip debugging through an SDI. This model does not require a dedicated external power source since it is intended to receive power from a PC, i.e., it is USB bus-powered.
This model supports SDI-1, SDI-2 and the newly developed SDI-3. It is a low-end model which is basic and economical, so does not support advanced debugging functions such as real-time tracing and time measurement.
M3T-PD32RM
Latest Ver.: V.3.01 Release 00
Released: Oct 1, 2006
Details of upgrade (See Tool News)
Operating Environment
The M3T-PD32R emulator debugger supports:
Window | Function |
---|---|
PD32RM Window | Controls entire debugger. You can perform the following basic debugging commands by using the tool bar buttons: program execution/stop, step execution, execution up to cursor position, and break point setting/cancel. You can also open various other windows from this window. |
Program Window | Displays the program. Source code is editable here. Matching address line is displayed in color for the program counter (PC). You can select display format from among "source", "disassemble" or "mixed". You can also set or cancel break points. |
Source Window | Displays the designated place of a program. Source code is editable here. Unlike the program window, you can open more than one window. The window is displayed continuing a certain function or task, and is convenient when break points have to be set and canceled repeatedly. |
Register Window | Displays/changes content of flags and registers particular to the MCU. |
Memory Window | Displays the contents of contiguous memory in dump format with "address" and "label". Can be displayed in binary, decimal, hexadecimal, and ASCII. Allows to modify the contents of memory, and also to fill and move specified blocks of memory. |
ASM Watch Window | Monitors changes in memory content and variable content declared on the assembly language level. Display format can be selected from among binary, decimal, and hexadecimal. |
C Watch Window | Displays C variable content. In addition to a window that displays variable formula of your choice, there are windows that display external variables, local variables within a file, and local variables within a function. |
Call Stack Window | Displays function call information of C language. |
Script Window | Window for executing commands from the keyboard or script files. An area is provided for displaying command execution results and command history. Execution results can be output to a file. |
S/W Break Point Setting Window | For setting/canceling software break points. Can set 64 break points maximum (OR condition). |
Window | Function |
---|---|
Trace Point Setting Window * Available for M32100T5-SDI-E and M32100T3-SDI-E. |
Sets/clears trace points. As a condition, combination of 6 trace points and each event can be set. |
Trace Window * Available for M32100T5-SDI-E and M32100T3-SDI-E. |
Displays the results of real-time tracing in the emulator. The following three display modes are supported: Bus mode, Disassemble mode and Source mode. Those modes can be used concurrently. |
Data Trace Window * Available for M32100T5-SDI-E and M32100T3-SDI-E. |
Graphically shows the data access information on the results of real-time tracing. |
Task Trace Window * Available for M32100T5-SDI-E and M32100T3-SDI-E. |
Graphically shows task execution histories of programs using real-time OS. |
Task Analyze Window * Available for M32100T5-SDI-E and M32100T3-SDI-E. |
Shows the results of statistical processing of measured data within the range specified with the Task Trace Window. This window shows the occupancies of tasks in a CPU. |
MR Window | Shows the state of the real-time OS M3T-MR32R. |
MR Trace Window | Graphically shows task execution histories of programs using the real-time OS M3T-MR32R (V.3.10 or later). Also, each history of interrupt handling and system call issuing is shown together. |
MR Analyze Window | Shows the results of statistical processing of measured data in the range specified with the MR trace window. And shows the list of the following records : the occupation status per interrupt handler or task, history of system call issuing. |
Time Measurement Window * Available for M32100T5-SDI-E and M32100T3-SDI-E. |
Sets time measurement conditions and references the measurement results. As the measurement results, the execution time (Max, Min, Average) and the measurement count are displayed. The number of measurement points are as follows : M32100T5-SDI-E : Up to four points M32100T3-SDI-E : One point |
GUI Input Window | Shows key input panels of user target system. You can make virtual key input buttons by simple mouse operation. While the program is running, pressing the button generates data input. |
GUI Output Window | Shows output panels of user target system. You can make virtual output LEDs or labels by simple mouse operation. |
Item | Description | |
---|---|---|
MCU supported | M32R Family M32R/ECU Series :
|
|
Emulation memory Capacity | RAM used as emulation memory. Note1 | |
Software break | Implemented by internal resource of MCU or instruction replacement. Note1 | |
PC Interface | USB 1.1, full-speed | |
Connection type for target board | JTAG connection | |
Target I/F | MCU control interface connector : 10-pin (2.54mm-pitch 5 times 2 sequences) |
|
Target host PC (OS) | Refer to Operating Environments of Products. | |
Power supply | Supplied from the host machine | |
External dimensions(main body) | Width | 61 mm |
Depth | 86.5 mm | |
Height | 22 mm | |
Weight | 130 g | |
Ambient environment condition (When operating) | Temperature humidity | 5 to 35 oC, 20 to 80% |
Dust and dirt | General office environment | |
Ambient environment condition (When stored) | Temperature humidity | -10 to 60 oC, 0 to 90% |
Dust and dirt | General office environment | |
Overseas standards | European Standards: EN 55022 Class A, EN 55024 US FCC Standard: FCC part 15 Class A |