Motors are everywhere; drive them efficiently
As the industry strives to improve the efficiency of motor drives, it is crucial to comprehend the types and characteristics of various motor technologies.
As the industry strives to improve the efficiency of motor drives, it is crucial to comprehend the types and characteristics of various motor technologies.
Renesas has successfully developed the core technologies of a dynamic circuit-based ultra-low power discrete-time (DT) delta-sigma (DS) ADC.
为了满足汽车E/E架构发展衍生的市场需求,我们将通过增加介于RH850/F1K系列和RH850/F1KM-S4系列之间的RH850/F1KM-S2系列产品以拓展客户的选择面。
半导体技术工艺节点是衡量芯片晶体管和其他组件尺寸的标准。这些年来,节点的数量一直在稳步增加,导致计算能力也相应增加。一般来说,工艺节点越小,特征尺寸越小,晶体管越小,速度越快,越节能。
执行役员兼High Performance Computing Analog & Power团队总经理片冈健,受邀作为嘉宾参加在台湾举办的COMPUTEX & InnoVEX 2023 研讨会,并进行了演讲。
Easy-to-use Software to Auto-Detect the Industrial Ethernet Protocol and Load the Corresponding Protocol Application
Radar modules require efficient antennas, which radiate the FMCW radar signal from the transceiver and receive the echoes created by the obstacles in the environment.
Introducing a high-speed simulator for R-Car S4, the Renesas QEMU Environment.
随着电子设备的电源要求不断提高,高效的电源管理已成为一种必要,而Power MUX负载开关是有助于有效进行电源管理的创新解决方案之一。